Input range is under range

The value is less than the minimum value allowed in the defined input range for this device. Depending on the device, the lowest acceptable signal in range is 0 mA or 4 mA.
Enter a value within the input range for this device, and then apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal