Deadband is over range

The deadband value is greater than half the distance between the low and high alarm limits. To resolve this error:
  1. In the
    Alarms
    view, subtract the
    Low Limit
    value from the
    High Limit
    value, and then divide the result by two.
  2. In
    Deadband
    , enter a number lower than the result of the calculation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal