Unlatch error

The unlatch service failed. Possible causes are:
  • A time out error occurred.
  • The message was sent to the wrong device.
  • There is no connection to the device.
Check your configuration, make changes as needed, and then save your changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal