Deadband illustration

This illustration of deadband shows the input data that sets each of the four alarms at some point during device operation. In the illustration, latching is disabled; therefore, each alarm turns Off when the condition that caused it to set ceases to exist.
1756
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal