Copy channel configuration

Use
Copy Channel Configuration
to copy the channel's properties to multiple channels on a device.
To copy channel configuration
  1. On the tab for the device, expand
    Channels
    , and then perform one of these actions as needed:
    • Select the appropriate individual channel.
    • Expand
      ChX
      and select
      Alarms
      or
      Limits.
  2. Select
    Copy Channel Configuration
    .
  3. In
    Copy Channel Configuration
    , select the checkboxes of the channels to which the copied properties applied.
    TIP:
    Use
    Uncheck All Channels
    to clear the selection of all channels.
  4. Select
    OK
    to finalize the changes and exit the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal