CJ Channel view

Use the
CJ Channel
view to configure the Cold Junction (CJ) parameters when a channel is configured for Thermocouple operation.
Use the
CJ Channel
view to:
  • Disable cold junction compensation to prevent the cold junction temperatures from being returned to the controller.
  • Enter a cold junction offset value as additional control over the cold junction behavior.
  • Specify the type of cold junction compensation the device uses.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal