Results - Measure and Record Values - High Reference

The device reads the value for the enabled channels.
  • If the reference signal is within the acceptable range, the status reads
    OK
    . Select
    Next
    to continue.
  • If the reference signal is not within the acceptable range, the status reads
    Error
    . Measure and enter the recorded reference values again for the channels in error. When a correct value is entered, the status shows
    OK
    .
You can also select
Cancel
to exit
Calibration Wizard
leaving the calibration status for that channel with an Error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal