Output Reference Signals - High Reference (Volts)

The output device starts to send high reference signals on all the selected voltage channels. These parameters are available in
Output Reference Signals - High Reference (Volts)
.
Parameter
Description
Channel
Shows the channels available to calibrate.
Calibrate
Identifies the channels selected in the previous window.
Calibration Range
Shows the High Reference Signal value that the device produces based on channel configuration. The calibration range shows -10 V to 10 V for Voltage.
High Reference
Shows the High Reference Signal value that the device produces. For voltage channels, the value is 10 V.
Back
Returns to the previous wizard window.
Next
Starts producing the reference signal on the selected channels.
Stop
Stops the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal