Attach Low Reference Signals

Attach a Low Reference source to the selected channels.
Attach Low Reference Signals
includes these parameters:
Parameter
Description
Channel
Shows the channels available to calibrate.
Calibrate
Identifies the channels selected in the previous window.
Calibration Range
Shows the value currently configured for the channel.
  • For the 1756-IF8I device:
    • The calibration range shows 0 mA to 20 mA when the
      Input Type
      is Current.
    • The calibration range shows -10 V to 10 V when the
      Input Type
      is Voltage.
  • For the 1756-IR12 device, the calibration range shows 0 Ohms to 500 Ohms when the
    Input Type
    is RTD.
  • For the 1756-IRT8I device:
    • The calibration range shows 0 Ohm to 500 Ohms when the
      Input Type
      is RTD.
    • The calibration range shows -100 mV to 100 mV when the
      Input Type
      is Thermocouple.
  • For the 1756-IT16 device, the calibration range shows -100 mV to 100 mV when the
    Input Type
    is Thermocouple.
Low Reference
Shows the low reference signal value to apply to the channel.
  • For group input calibration or one at a time input calibration for 1756-IF8I channels, the value is 0 V for Voltage and 4 mA for Current.
  • For group input calibration or one at a time input calibration for 1756-IRT8I channels, the value is 0 mV for Thermocouple input signals and 0 Ohm for RTD input signals.
Back
Returns to the previous wizard window.
Next
Continues the process.
Stop
Stops the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal