Specify device output behavior when communications fail in Program Mode

Select the behavior of the outputs of non-isolated analog output devices if communication fails in Program mode.
IMPORTANT:
Outputs always go to Fault mode if communications fail in Run mode.
To specify device output behavior when communications fail in Program Mode
  1. On the tab for the device, select
    Channels
    .
  2. In the
    Channels
    view, select one of these options:
    • Leave outputs in Program Mode state
    • Change outputs to Fault Mode state
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal