Unlatch service failed
The unlatch service failed. Possible causes are:
- A time out error occurred.
- The message was sent to the wrong device.
- There is no connection to the device.
- The alarm condition is not configured to latch when an alarm is triggered.
Check the configuration, update the value, and apply the changes. Also verify the device is the correct catalog and has a connection established.
Provide Feedback