Specify the input range for each channel

Use the
Channels
view to specify the input range for each channel.
To specify the input range for each channel
  1. On the tab for the device, select
    Channels
    .
  2. In the
    Channels
    view, in the
    Input Range
    column, select the appropriate current or voltage operating range for each channel.
  3. Select
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal