Specify a Real Time Sample period
Use the
Channels
view to specify the Real Time Sample (RTS) period for the device. The RTS rate specifies how often the analog input device samples the incoming data.To specify a RTS period
- On the tab for the device, selectChannels.
- In theChannelsview, inReal Time Sample (RTS), enter the input sampling period in milliseconds.
- SelectOKto save the changes.
Provide Feedback