Specify the Real Time Sample period
Use the
Input Channels
view to specify the Real Time Sample (RTS) period for the device. The RTS rate specifies how often the analog input device samples the incoming data. Use the ChX
view to configure each channel.To specify the RTS period
- On the tab for the device, selectInput Channels.
- In theInput Channelsview, inReal Time Sample (RTS), enter the time (in milliseconds) to indicate how often the device inputs are to be sampled.
- (optional) SelectSynchronize sampling with other devicesto synchronize the time at which samples are taken for all 1756-IF4FXOF2F devices in a rack.
Provide Feedback