Start device calibration
Calibrate device inputs and outputs to obtain optimum accuracy. The application calibration screens guide you through the entire process.
Prerequisites
- Verify the controller is online and in Program mode.
- Stop the process your output device is controlling or your input device is tracking. Control may be impaired during the calibration process.
- Disconnect input signals and connect test signals. Any control that depends on the normal input signals does not have them during the calibration process.
- Disconnect output signals and connect a suitable measuring instrument. Any control that depends on the outputs from this device does not have them during the calibration process.
- 1756-OF4 and 1756-OF8 devices can be calibrated in multiple input ranges. Select the appropriateOutput RangeorInput Rangein the configuration views.IMPORTANT:
- Entering calibration causes all input channels to freeze at their current values and fault. Control may be impaired.
- Calibration interacts directly with the device overruling any controller that may be trying to use the device.
- Control may be impaired by the calibration process.
- When you begin the calibration process, if a real-time connection is currently open, all device points fault.
To start device calibration
- On the tab for the device, selectCalibration.
- In theCalibrationview, selectStart Calibration.
Provide Feedback