Select device channels to calibrate

Select one or more device channels to calibrate. You can calibrate any combination of channels in groups or calibrate all channels at once. It is recommended that you calibrate all of the channels on your device each time. This helps maintain consistent calibration readings and improve device accuracy.
To select device channels to calibrate
  1. On the tab for the device, select
    Calibration
    .
  2. In the
    Calibration
    view, select
    Start Calibration
    .
  3. In
    Calibration Wizard - Select Channels to Calibrate
    , select the
    Calibrate
    checkbox for each channel to calibrate.
  4. Select the method of calibration:
    • Calibrate channels in groups.
      Applies a reference signal to all of the selected voltage channels at the same time, and then to all of the current channels at the same time.
    • Calibrate channels one at a time.
      Applies a reference signal to one channel at a time, waits for you to record the results, and then continues to the next channel.
  5. Select
    Next
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal