Device being used for control. Device identity mismatch.
Calibration should not be performed on a device that is currently being used for control. All channels freeze at their current values, and control may be interrupted. Read and understand the important information before continuing with calibration.
IMPORTANT:
- Calibration disconnects the device from the control signals to which it is normally connected and connects it to reference signals.
- During calibration, output devices do not update their outputs with the data values requested by the controller. Outputs may transition based on the calibration process itself if that channel is being calibrated.
- During calibration, the controller is not receiving measurements of signals, originating in the system under control, from the input device.
In addition, a mismatch between the device in the software and the actual physical device exists. To stop the calibration process, select
Cancel
.Provide Feedback