Descrip: RTS

Specifies how often, in milliseconds, the device scans its input channels. After the channels are scanned, the device multicasts the data.
The selected Real Time Sample (RTS) period applies to the entire device. You cannot set a different value for each channel.
The RTS period controls how often the device prepares new readings. The Requested Packet Interval (RPI) controls how often the device sends its current readings to the controller. Ideally the RTS and RPI should be identical so that each reading is sent to the controller only once at the time of sampling.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal