Loading
Product Spotlight | September 27, 2024

Rockwell Automation Brings New Wireless Interfaces, New Edge to Stratix® 4300

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
  4300 Wireless Router, 1783-RA, Full product line

The Stratix® 4300 Remote Access™ Router solution now has both Wi-Fi and LTE (cellular) wireless options available. These options include Ethernet only (existing product with 2 or 5 ports), Ethernet and Wi-Fi (2 or 5 ports), Ethernet and LTE (2 or 5 ports), and Ethernet, Wi-Fi, and LTE (2 or 5 ports).

The addition of these wireless interfaces for Wi-Fi and LTE (cellular) allows customers to use the Stratix 4300 in applications where a physical Ethernet connection may be difficult or not desired. Wireless options on the Stratix 4300 router help users reduce downtime, maintain business continuity, and enable a productive workforce.

Stratix 4300 will continue to be a dedicated platform for the FactoryTalk® Remote Access™ solution, which enables VPN connectivity with industrial networks, for increased visibility across your plant. All Stratix 4300 units come pre-installed with FactoryTalk Remote Access.

Supporting accessories such as antenna and mounting options are available to plants with flexible locations for their Stratix 4300.

Some of the distinct benefits to running FactoryTalk Remote Access with the Stratix 4300 include a NAT 1:1 for routers which maps an internal address (LAN) to an external address (WAN or VPN) and the ability to conduct remote updates, allowing customers to use FactoryTalk Hub™ to update the Stratix 4300.

Allen-Bradley®, Stratix®, Stratix® 4300, and Rockwell Automation are trademarks of Rockwell Automation, Inc.

Published September 27, 2024

About Rockwell Automation

 
 

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more pr oductive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 26,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2025. To learn more about how we are bringing the Connected Enterprise® to life across industrial enterprises, visit www.rockwellautomation.com.

About the Rockwell Automation PartnerNetwork

Rockwell Automation believes we're better together—and we do our part by delivering an expansive, global partner ecosystem of market-leading technology, superior support and services, and an integrated and streamlined approach to business. Succeed on an international scale by utilizing our network's breadth of innovative technologies and services that no single vendor can provide alone. To learn more about how the PartnerNetwork is helping to deliver the value of The Connected Enterprise, visit PartnerNetwork Program.


Topics: FactoryTalk Remote Access
Related News
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation Brings New Wireless Interfaces, New Edge to Stratix® 4300