Loading
Press Release
Recent ActivityRecent Activity

Rockwell Automation Industrial Computers, Thin Clients Enhanced for Use in Hazardous Locations and Harsh Environments

New certifications and conformal coat options help protect product longevity and production uptime

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Rockwell Automation Industrial Computers, Thin Clients Enhanced for Use in Hazardous Locations and Harsh Environments hero image

Industrial producers can now improve the reliability and longevity of their automation systems in hazardous locations.

Rockwell Automation has enhanced two of its modern visualization solutions, the Allen-Bradley VersaView 5200 thin clients and VersaView 5400 industrial computers, for use in harsh locations in industries like oil and gas, tire and rubber, and pulp and paper.

Both products are now certified for use in UL Class I Division 2 and ATEX Category 2 hazardous-area applications. In addition, the products carry a BIS certification for markets in India. The products are available with these new certifications at no added cost to customers.

Both products are also now available with conformal coat options. Conformal coating helps protect product circuitry from environmental stresses like moisture, fungus, dust and corrosion.

When used with ThinManager software from Rockwell Automation, VersaView 5200 thin clients can start receiving information as soon as they’re plugged in. Device configuration is not needed, resulting in faster device replacement. And because information is stored on a server instead of locally, sensitive information is less likely to be lost if a VersaView thin client goes offline.

VersaView 5400 industrial computers use an open-architecture design to give producers the freedom to install software that suits their needs. They also serve as an appliance within the FactoryTalk Analytics for Devices software from Rockwell Automation. This combined hardware and software package gives users access to health and diagnostics data for smart devices to help track and improve their performance.

Published December 2, 2020

Topics: Thin Clients Industrial Computers & Monitors

About Rockwell Automation

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more productive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 25,000 problem solvers dedicated to our customers in more than 100 countries. To learn more about how we are bringing The Connected Enterprise to life across industrial enterprises, visit www.rockwellautomation.com.


Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left VersaView approved for use in harsh environments