Loading
Press Release | May 20, 2025

Rockwell Automation Launches EtherNet/IP In-cabinet Solution to Help Manufacturers Build Smarter, More Efficient Panels

New offering can cut wiring time by up to 80%, speeding production and innovation

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
One single-pair EtherNet/IP In-cabinet flat media cable using 1486 Connectors to link a 1834 gateway, E100 Electronic Overload Relay, 100-E Contactor, 140MT Motor Protection Circuit Breaker, and three push buttons.

MILWAUKEE, Wis., May 20, 2025—Rockwell Automation, Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and digital transformation, today announced the release of its EtherNet/IP™ In-cabinet Solution, a major advancement designed to meet the growing demand for smarter, faster and more connected manufacturing operations.

As companies strive to improve productivity and reduce downtime, traditional hard-wired control panels often stand in the way, limiting data access and complicating system upgrades. The EtherNet/IP In-cabinet Solution addresses those challenges by streamlining communications between devices with the panel, making system integration simpler, boosting real-time data access and helping manufacturers make faster, more informed decisions.

"Our EtherNet/IP In-cabinet Solution is a game-changer in industrial connectivity," said Kelly Passineau, product manager at Rockwell Automation. "By leveraging single-pair Ethernet/IP technology, we're helping customers reduce installation time, enhance operational efficiency and integrate wired components into a more intelligent, data-driven network.”

Early adopters are already seeing the impact. Volga, a Rockwell Systems Integrator Partner and a leading manufacturer based in Brazil specializing in electrical, mechanical and automation control, reported dramatic improvements after adopting the EtherNet/IP In-Cabinet Solution.

"The EtherNet/IP In-cabinet Solution reduced our assembly time by over 65%, enabling us to wire starters and panel operators in just over an hour," said Carlos Leopoldo, commercial director at Volga. "Beyond the significant time savings, this system provides numerous benefits for our panel builders, including space efficiency, customizable panel operator colors, a reduction in SKUs, minimized risk of incorrect connections and more straightforward inspections. It’s a well-designed solution that enhances efficiency and reliability for both panel builders and end users who can benefit from improved communication, diagnostics and easier maintenance.”

Key benefits of this new offering include:

  • Faster Installation: When implemented in accordance with recommended standards, it can help cut wiring time by up to 80% compared to traditional hard-wired installation.
  • Optimized Space: The compact design allows for efficient use of cabinet space, enabling more devices to be installed in the same footprint and reduces overall panel size.
  • Improved Data Access: Boost productivity with quick, real-time communication between devices.
  • Scalability: Easily expand and adapt to future networking needs without major infrastructure changes.

Additionally, a plug and play design enables easy configuration, commissioning and maintenance, ultimately reducing disruptions to production schedules.

Learn more about the EtherNet/IP In-cabinet Solution on Rockwell’s website.

Published May 20, 2025

About Rockwell Automation

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more pr oductive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 26,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2025. To learn more about how we are bringing the Connected Enterprise® to life across industrial enterprises, visit www.rockwellautomation.com.


Media Contacts

Michelle Stange
Michelle Stange
Public Relations Lead, Rockwell Automation
Connect:
EmailEmail

Topics: EtherNet IP Network Ethernet IP In-cabinet Solution
Related News
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Automation Launches EtherNet/IP In-cabinet Solution to Help Manufacturers Build Smarter, More Efficient Panels