Loading
Product Spotlight | February 20, 2024

Rockwell Automation Offers Groundbreaking Solutions for Control Software Optimization with Embedded Edge Compute Modules

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

The Embedded Edge Compute Module builds on Rockwell Automation’s recent history of enabling PC or compute functionality with the power of Logix. This Edge solution provides key scalability and remote support functions to today’s workforce. At first release, the Embedded Edge Compute enables FactoryTalk® Optix™ software and provides a communication path to REST API, OPC UA and MQTT to meet the needs of a variety of applications.

Embedded Edge Compute Modules are one of the solutions in the new FactoryTalk Optix portfolio. The FactoryTalk Optix portfolio allows users to choose their own technology mix, where for the first time, Rockwell Automation customers can use visualization software to design HMI applications that can natively work with both Rockwell Automation and third-party controllers and display a choice of hardware from either Rockwell Automation or a third-party. Users can connect to a variety of third-party software, devices or systems using software designed for interoperability and full OPC UA support. Users also only pay for the features they need with runtime licensing that is based on the capabilities in their application.

Click here to learn more about Rockwell Automation’s FactoryTalk Optix portfolio.

Published February 20, 2024

About Rockwell Automation

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more productive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 27,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2024. To learn more about how we are bringing the Connected Enterprise to life across industrial enterprises, visit www.rockwellautomation.com.


Media Contacts

Mario Martin
Mario Martin
Senior Manager, Global Public Relations, Rockwell Automation

Related News
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right
  5. Chevron LeftChevron Left Rockwell Automation Offers Groundbreaking Solutions for Control Software Optimization with Embedded Edge Compute Modules Chevron RightChevron Right