Loading
Product Spotlight | September 16, 2024

Rockwell Automation Simplifies Installation, Increases Productivity with New Panel-mount, High-power VFD Option

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
PowerFlex 755TS Frame 7A left side

PowerFlex 755TS Frame 7A drive

Industrial companies can simplify installation, increase productivity and maximize uptime with Allen-Bradley® PowerFlex® 755TS frame 7A drives with TotalFORCE® technology. PowerFlex 755TS six-pulse drives provide more power in a smaller footprint and allow companies—especially with heavy industry applications—to get the most out of space and investments.

The PowerFlex 755TS frame 7A low voltage drive expands the power range up to 500 Hp (355 kW) and provides a new panel-mount solution for high horsepower applications. It's 75% smaller than floor mount alternatives, making it easier to install and meet premium footprint requirements. 

Additionally, the PowerFlex 755TS frame 7A drive enables easier maintenance and commissioning for system integrators and OEMs in industries like oil and gas, power generation, water/wastewater, and mining and metals. This portfolio addition brings a simplified and consistent user experience to virtually any motor control application. This includes traditional fan, pump and conveyor applications. It also includes more advanced motor control processes that require high-performance features typically found in specialized drive solutions.

Published September 16, 2024

About Rockwell Automation

 
 

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more pr oductive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 26,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2025. To learn more about how we are bringing the Connected Enterprise® to life across industrial enterprises, visit www.rockwellautomation.com.

About the Rockwell Automation PartnerNetwork

Rockwell Automation believes we're better together—and we do our part by delivering an expansive, global partner ecosystem of market-leading technology, superior support and services, and an integrated and streamlined approach to business. Succeed on an international scale by utilizing our network's breadth of innovative technologies and services that no single vendor can provide alone. To learn more about how the PartnerNetwork is helping to deliver the value of The Connected Enterprise, visit PartnerNetwork Program.


Related News
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Rockwell Offers New Panel-mount, High-power VFD