Loading
Press Release | March 10, 2016
Recent ActivityRecent Activity

New Controller From Rockwell Automation Simplifies Machine Safety

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Compact GuardLogix 5370 controller provides integrated safety and motion on single EtherNet/IP network

MILWAUKEE, March 10, 2016 — Manufacturers and equipment builders are looking for ways to simplify and standardize safety across their machines and systems. With the new Allen-Bradley Compact GuardLogix 5370 controller from Rockwell Automation, users no longer need separate networks and controllers for safety and motion in applications with up to 16 axes. This makes it easier to design safety into a wide range of standard and custom machines, and results in simpler system architectures.

“The new Compact GuardLogix 5370 controller has all the performance capabilities of our popular Allen-Bradley CompactLogix 5370 controller, while also providing integrated safety and motion on a single EtherNet/IP network,” said Ming Jing Ye, global product manager, Rockwell Automation. “When safety, motion and standard control are combined into one package, configuration is easier, wiring is reduced and users get better diagnostics. Ultimately, it helps increase machine uptime and plant productivity.”

The Compact GuardLogix 5370 controller also helps users meet global safety standards. It achieves Safety Integrity Level 3, Performance Level e and Category 4 – the highest ratings for machine safety. When used in combination with the Allen-Bradley Kinetix 5500 servo drive or the Allen-Bradley PowerFlex 527 AC drive, users have integrated safe torque off on EtherNet/IP.

As with other Logix controllers, engineers use the Rockwell Software Studio 5000 software to configure the Compact GuardLogix 5370 controller and develop all elements of their control system. Data can be defined once, and then easily accessed and re-used across different machine types to speed system development and commissioning.

In addition, a single programming environment for both safety and standard control removes the need to manually manage separate standard and safety memory, or partition logic to isolate safety.

The Compact GuardLogix 5370 controller, being manufactured in Singapore, also includes dual Ethernet ports to support both linear and device-level-ring (DLR) network topologies. Built-in energy storage removes the need for batteries, and a removable 1-GB Secure Digital (SD) card improves data integrity.

Rockwell Automation also will be releasing an on-machine option later this year – the Allen-Bradley Armor Compact GuardLogix 5370 controller. This option allows users to place the controller closer to the application or onto the machine, which eases installation, commissioning and troubleshooting. The on-machine controller is IP67-rated for wash-down protection and includes quick-connect cabling to ease system wiring.

News Release Assets
Image available upon request or here at box.com.

About Rockwell Automation 
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts
Paul Whitney
Rockwell Automation
414.382.3696
pwwhitney@ra.rockwell.com

Leanne Hanson 
PadillaCRT
612.455.1776
leanne.hanson@padillacrt.com

Allen-Bradley, Armor, CompactLogix, GuardLogix, Kinetix, LISTEN. THINK. SOLVE., PowerFlex, Rockwell Software and Studio 5000 are trademarks of Rockwell Automation Inc.
EtherNet/IP is a trademark of ODVA Inc.

 

Published March 9, 2016


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left New Controller From Rockwell Automation Simplifies Machine Safety