Loading
Press Release | May 21, 2020
Recent ActivityRecent Activity

Enhanced Communication Module Provides Additional Resiliency

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail

Industrial producers can now improve their network resiliency by using primary and backup adapters for the 1756-EN4TR ControlLogix® EtherNet/IP communications module. This new redundant-adapter functionality is provided through a recent firmware update to the communication module.

In addition to helping users improve network redundancy, the module’s firmware enhancement also offers more advantages:

  • No single point of failure: When used with ControlLogix controllers and redundant switches, the communication module is no longer a single point of failure. This can improve uptime and productivity in continuous process applications like oil and gas.
  • Architecture options: The firmware enhancement can be used with a single ControlLogix controller or redundant controllers. It can also be used with star or Device Level Ring (DLR) architectures. This gives users design flexibility.
  • Ease of modification: An existing 1756 I/O chassis can be modified for redundant adapters. Slots 0 and 1 are used for the redundant adapters.

The 1756-EN4TR communication module implements network-based access control for users, devices and networks in a 1756 ControlLogix chassis. The module can increase performance in networked operations, with 1-gigabit-per-second communications speeds and the ability to support future network or infrastructure expansions.


Click to download image.

ControlLogix® is a trademark of Rockwell Automation Inc.

Published May 21, 2020


  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right