In this video from 2018 PACK EXPO International, LinMot USA highlights three products with new features: its C1250 EtherNet/IP™ low-voltage, modular, single-axis servo drive, programmed in the ControlLogix® Studio 5000® environment with added features for CIP Sync™; its E-guide unit for linear motors that provides more carriage rigidity for moving stator applications; and linear motors and guides designed for IP69K hygienic applications, with new liquid cooling for its motors.
LinMot manufactures linear motors and servo drives for harsh environments, and guided actuators and magspring constant-force magnetic springs.
Watch the video above to see the technology demonstrations.
The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.