Loading
Case Study
Recent ActivityRecent Activity

Solutions in Action: AFA Systems

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail
Lockheed Martin Aeronautics, Fort Worth, Texas.  10/31/2008.  EMAS 2 and 3 and MOVING LINE 1 thru 4 for f-35.
Case Study
Recent ActivityRecent Activity
Solutions in Action: AFA Systems

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail

Solutions

  • Allen-Bradley CompactLogix Multi-Axis Servo Drive
  • Allen-Bradley Kinetix 2000
  • Allen-Bradley 6000 Multi-Axis Servo Drive

When a leading manufacturer of powdered baby formula required secondary packaging equipment for their Jakarta, Indonesia facility, they turned to an innovative supplier half a world away. Ontario-based AFA Systems provides custom engineered and fully integrated end-of-line packaging solutions to meet exacting – and oftentimes unique – specifications. AFA Systems' portfolio extends from horizontal and vertical cartoning and case packing machines to palletizing and specialty solutions. The machine builder has been serving the food and beverage, pharmaceutical and consumer packaged goods industries for more than 60 years.

The company's Jakarta customer required a two-fold packaging system for its powdered milk application: an integrated cartoner and case packer. AFA Systems delivered a solution based on its new MK-BIB autoload cartoner and TR-QCP Transrector™ robotic case packer. As bags of milk powder come off two vertical form fi ll seal (VFFS) machines, it enters the MK-BIB cartoner's dual servo starwheel infeed system. At a rate of 150 cartons a minute, the bags are accurately placed in continuous motion buckets, which then load the point-of-purchase cartons. After sealing, the cartons travel downstream via a 10-foot conveyor to the case packer. At the TR-QCP case packer, cartons are choke-fed to a servo-driven starwheel upender. The upender correctly positions the cartons for loading, and a robotic end-loading tool places the cartons in the case. Unlike typical end-of-arm tools (EOAT) that use vacuum generators and compressed air to pick and place cartons, this device utilizes a clamp mechanism. Since the tool does not use compressed air, it saves a signifi cant amount of energy.

“Machine fl exibility was the most challenging aspect of the project,” explained Eric Langen, sales and marketing representative, AFA Systems. “We had to build a solution that could handle multiple packaging parameters and materials.” On the cartoning equipment, the system accommodates two sizes – one for 400 grams of product delivered in one bag and the other for 1800 grams of product delivered in two 900-gram bags. In addition, the machine can run chipboard cartons for the smaller packages and corrugate for the larger ones. The case packing equipment is equally flexible and can deliver either six or 24 cartons per case. “To optimize throughput, our customer required a very short changeover time between confi gurations,” Langen said. “They also needed to conserve space on their plant floor.” A Rockwell Automation control and information solution enabled AFA Systems to achieve application fl exibility – in a small footprint. An Allen-Bradley® ControlLogix® programmable automation controller manages all machine and motion functions. For motion synchronization, the controller is tightly integrated with Allen-Bradley Kinetix® 6000 and Kinetix 2000 multi-axis servo drives.

Allen-Bradley Guardmaster® safety relays help providemachine and personnel protection. The system is integrated on EtherNet/IP™ and monitored on PanelView™ Plus 700 graphic terminals. “The compact servo technology helped us signifi cantly reduce size,” said Langen. “Our system's minimal footprint was a key diff erentiator for us.” Impressive changeover times also set AFA Systems apart. While typical machines require 40 to 50 minutes for changeover, this custom solution can complete the process in less than half that time. “Operators can make most of the adjustments right through the control system's human machine interface (HMI),” Langen explained. “As a result, our machines achieve some of the fastest changeovers in the industry. We can build systems that are ready to run new product in two minutes.”

With the initial installation in place, AFA Systems plans to expand the customizable solution to its home market in North America and other regions around the world. “Globally, Rockwell Automation is a recognized and respected brand,” said Langen. “As a Rockwell AutomationMachine Builder Partner, we've standardized on Rockwell Automation systems. That gives our large, multinational customers added confi dence – wherever their plants are located.” Allen-Bradley, ControlLogix, Guardmaster, Kinetix, and PanelView are trademarks of Rockwell Automation, Inc. EtherNet/IP is a trademark of ODVA. Transrector is a trademark of AFA Systems Ltd.

For more information: Eric Langen, Sales and Marketing Representative AFA Systems, Inc. Phone: 905.456.870, Ext. 244 Email: eric.langen@afasystemsinc.com

Published August 1, 2014

Tags: Food & Beverage, Household & Personal Care
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Case Studies Chevron RightChevron Right