Loading
Case Study | INDUSTRIAL ANALYTICS/MINING/FACTORYTALK ANALYTICS
Recent ActivityRecent Activity

Polyethylene Producer Increases Production

A Large Chemical Manufacturer Reduces Transition Time and Increases Production with Advanced Process Control

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Aerial view of twilight of oil refinery ,Shot from drone of Oil refinery and Petrochemical plant at dusk

Challenge: Maximize Production and Profit Across the Entire Manufacturing Lifecycle

Operating in many countries, the chemical manufacturer is one of the largest integrated energy companies in the world. The Polyethylene business unit is a leading producer of polyethylene with a full range of low-density polyethylene (LDPE) and linear low density polyethylene (LLDPE) products for the packaging, agricultural, consumer goods, and construction sectors.

Chemical laboratory technicians fitting hose
 

Unlike traditional, large-scale petrochemical manufacturers that focus on a single product, polymer manufacturers produce many products over a wide range of conditions. Operating a polymer reactor to meet these varying specifications is a complex, non-linear control problem. As a result, operations must focus not only on maintaining the quality of each product during “at-grade” conditions, but also on transitioning from one grade to the next in the most time- and cost-efficient manner. To maximize production and profit across the entire production lifecycle, manufacturers must continuously control the many variables that influence product quality and production rate.

The customer’s European unit makes a wide range of product grades and produces hundreds of thousands of kilotons of linear low-density polyethylene (LLDPE) per year, using its propriety process to produce the chemical. The customer needed a way to meet specific production targets, including increasing LLDPE production, reducing off-spec material, and reducing transition times between grades.

Solution: Making the Grade with FactoryTalk® Analytics™ PavilionX™

The company learned about the Rockwell Automation advanced process control (APC) solutions during a technical exchange meeting and was impressed with the company’s proven expertise in the polymer industry. Concluding that Rockwell Automation Solutions could help the company achieve its quality and production goals, the company implemented the Rockwell Automation FactoryTalk Analytics PavilionX solution.

FactoryTalk Analytics PavilionX combines steady-state optimization with model predictive closed loop control to reduce product variability and transition times, improve reactor stability, and maximize raw material efficiency.

Polyethylene, Plastic Clear Resin Pellets in a Holding Hand
 

The customer’s specific needs for the software included controlling the gas phase composition in the reactor and managing and controlling instantaneous reactor product quality and transitions between grades. FactoryTalk Analytics PavilionX creates online predictive models that augment hardware instruments and laboratory analyses to provide real-time estimates of process and product conditions. These virtual instruments provide the feedback and predictive process information needed to keep production on track and help prevent process upsets, identifying problems and providing answers quickly­—without the time and expense of additional lab analyses. The customer's specific requirements were to monitor main quality variables such as Melt Flow Index (MFI) and density from actual reactor data.

Results: Real Benefits, Real Savings—within Months

The first Rockwell Automation Solution was installed, implemented, tested, and commissioned at the customer site within 8 months. Rockwell Automation provided most of the engineering expertise with the support of customer personnel, who were trained during project execution.

The benefits of FactoryTalk Analytics PavilionX – including significant improvements in production levels, reduced disturbances, reduced reactor variance, and transition time savings—were quickly apparent to the customer. The customer also reduced the variability of product properties by 50 percent because of implementing Rockwell Automation software. “From this we could operate closer to our hardware constraints, resulting in higher throughput,” said a customer representative. The software also decreased transition times by up to 50 percent (depending on the LLDPE grade produced), increased production by seven percent, and increased efficiencies in monomer and catalyst use.

 
Key Benefits:

Reduced variability of polymer properties by 50%

Reduced transition times by 25-50%

Increased production by 7%

Increased efficiencies in monomer and catalyst use

According to the customer representative, the project was a success and delivered additional benefits, which enhanced the profitability of the plant by increasing the range of options.

"We gained non-APC-related improvements caused by a new understanding of the constraints of the systems. To me, one of the most remarkable improvements is the ability to run new grade transitions which were not possible using the old control scheme. This gives us a higher flexibility in reacting to the needs of our customers."
Customer Representative

Based on the success of the project, Rockwell Automation and the customer formed a strategic alliance to deploy Rockwell Automation advanced process control solutions in customer’s polyethylene facilities, its joint venture organizations, and its licensees worldwide. In the first two years of the alliance, the customer and its affiliated organizations have successfully deployed 14 projects with Rockwell Automation.

Published July 13, 2023

 
Topics: Chemical FactoryTalk Analytics
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Case Studies
  5. Chevron LeftChevron Left Reduce Cycle Time to Production
Please update your cookie preferences to continue.
This feature requires cookies to enhance your experience. Please update your preferences to allow for these cookies:
  • Social Media Cookies
  • Functional Cookies
  • Performance Cookies
  • Marketing Cookies
  • All Cookies
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose