Loading
Blog | Motor Control
Recent ActivityRecent Activity

How to Prevent MCC Corrosion with Insulated Bus Technology

Many industries have corrosive environments that can damage equipment. Learn how you can prevent MCC corrosion with insulated bus technology.

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail
Main Image
Blog | Motor Control
Recent ActivityRecent Activity
How to Prevent MCC Corrosion with Insulated Bus Technology
Many industries have corrosive environments that can damage equipment. Learn how you can prevent MCC corrosion with insulated bus technology.

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail

Many industries around the world face challenges with corrosive environments, whether it is inside their facilities with air pollutants such as sulfur dioxide, or outdoors with corrosive factors such as water and salt fog. Corrosion is the single largest cause of the breakdown of machinery, structures, supports, and motor control equipment in a plant.

Such demanding environments require that extra thought be given to equipment longevity and arc flash avoidance. When it comes to motor control centers, the power bus design can help address both. The horizontal bus on CENTERLINE Motor Control Centers (MCCs) can be insulated with a factory-installed polypropylene flame-retardant wrap that helps prevent arc propagation and prevents MCC corrosion by creating a resistant seal around the busbar.

The oil and gas industry, for example, can subject MCCs to harsh and corrosive environments. From harsh environments in the refineries to salt fog that is often experienced on offshore drilling platforms, the polypropylene wrap used in CENTERLINE 2100 MCCs with insulated bus provides resistance to the severe environments. The increased resistance to corrosion of the insulated busbar can lead to increased longevity and performance.

Arc Flash Reduction

A sound structural design and a well-supported, isolated bus system are critical for an MCC to withstand the effects of an arc flash event. The two side sheets on every MCC section and a robust bus support design significantly contribute to the ability of the equipment to contain and redirect the arc flash energy.

An arc flash event has the potential of expelling large amounts of energy that can have deadly consequences. The energy in the form of the arc flash can reach temperatures of 35,000 °F, which is hot enough to vaporize copper and aluminum cables and busbars. The explosion also creates high pressure and sound waves. These events can be triggered by equipment that could be underrated for the available fault current, by accidental contact with an energized conductor, or corroded equipment such as a busbar in an MCC. Insulating the busbar in an MCC and helping prevent arc propagation or accidental contact is important for personnel and equipment safety.

Equipment Longevity

The polypropylene wrap that surrounds and insulates the busbar also helps protect and extend the life of the MCC. The wrap protects the busbar from air pollutants such as:

Sulfur dioxide

Trace materials like oils and lubrications

Dust found in sawmills and other food processing facilities

Moisture and other caustic materials prevalent in a manufacturing facility

While you can’t always control your operating environment, you can select products that are designed to withstand its challenges.

Learn more about CENTERLINE motor control centers. 

Published September 2, 2020

Tags: Motor Control, Motor Control Centers, Low Voltage

Andrew Schaeffler
Andrew Schaeffler
Senior Product Specialist, Rockwell Automation
Andy Schaeffler has worked in customer-facing roles throughout his career at Rockwell Automation. He is passionate about providing solutions that bring value to all aspects of the project and help make our customers more successful.
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

When Did You Last Think About Your Motor Control Centres?
Main Image
Blog
When Did You Last Think About Your Motor Control Centres?

Motor Control Centres (MCCs) power just about every manufacturing facility in the world, but do these unsung heroes get the attention they deserve? And what is the cost of MCC failure?

Read Now
The Offshore Oil and Gas Facilities Lifecycle
Main Image
Blog
The Offshore Oil and Gas Facilities Lifecycle

Many oil and gas companies are looking to extend the lifecycle of their automation systems.

Read Now
Improve Oil and Gas Operator Effectiveness with a Modern DCS
Main Image
Blog
Improve Oil and Gas Operator Effectiveness with a Modern DCS

A modern DCS can help novice oil and gas operators perform like your best operators with actionable alarming, predictive insights and a high-performance HMI.

Read Now
  • Sales
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right