Loading
Blog
Recent ActivityRecent Activity

Digital Transformation through 5G standalone (SA)

Rockwell Automation and Nokia join forces to enable private 5G standalone (SA) for industrial transformation.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
A bearded male wearing protective equipement looks at a tablet on the manufacturing floor in a factory.

The collaboration between Rockwell Automation and Nokia is pivotal towards the digital transformation of industrial networks through private wireless. Together, we enhance industrial connectivity, improve operational efficiency, and increase network customization and security. The combination of Rockwell Automation’s industrial automation solutions and Nokia’s wireless technologies supports emerging technologies such as Industrial Internet of Things (IIoT), augmented reality (AR), and artificial intelligence (AI). These capabilities are vital for industries looking to innovate and stay competitive.

A key current focus for Nokia and Rockwell Automation is the use of licensed, or lightly licensed, spectrum as an enabler for private cellular performance and robustness. In the United States, Citizens Broadband Radio Service (CBRS) provides 150 MHz of lightly licensed spectrum for use with private LTE and 5G networks. This spectrum can be requested in 10 MHz increments and used at no cost. Additionally, guaranteed access to up to 20 MHz of spectrum can be purchased via Priority Access Licenses (PALs). Private 5G is validated and ready for industrial use today, with an increasing number of customers showing trust in 5G. Consequently, the adoption of 5G standalone (SA) and CBRS is a hotter topic than ever.

Nokia and Rockwell Automation have teamed up to evaluate private 5G SA networks using CBRS spectrum for real-time industrial control with EtherNet/IP™ protocols. This technology partnership enhances industrial connectivity, leveraging Nokia's robust 4G LTE and 5G technologies to optimize manufacturing operations with high-speed and reliable connectivity. Since EtherNet/IP™ is transported over TCP/IP, multiple automation devices can be supported behind a single wireless router, without any of the special tunneling or extra equipment that is currently required for other industrial Ethernet protocols.

By integrating industrial automation expertise from Rockwell Automation with wireless technology expertise from Nokia, the collaboration improves operational efficiency through greater automation, real-time data collection and analytics. This synergy streamlines processes, reduces downtime and increases overall efficiency. Additionally, the technology partnership helps ensure a secure and dedicated network infrastructure, crucial for industrial applications.

Nokia 5G Diagram

The above illustration is a simplified representation of the test bed that was used for the collaborative testing. It represents an untethered stationary industrial asset application use case, consisting of:

  • One area controller with a GuardLogix® safety controller
  • Two distributed areas with FLEX 5000® standard and safety I/O, representing skids, machines or equipment

(Note: the purpose of the safety controller in each distributed area was to collect test bed telemetry data only).

A Nokia private solution was used, comprised of:

  • 5G radio access network (RAN), 3GPP Release 15, 5G SA and operating in n48 spectrum band (CBRS). Nokia AirScale baseband unit (BBU), two AZQC AirScale radio units (RUs).
  • 5G core (5GC) operating in DAC on-premise Mission-Critical Industrial Edge (MXIE) server
  • Two FRRO501c industrial 5G SA routers (in cellular parlance, user equipment or UEs)

Tests were run according to a well-established test plan provided by Rockwell Automation with strict success criteria of zero connection faults over a limited 3-hour test period. The test plan included a series of test cases to establish reliable EtherNet/IP standard and safety (CIP Safety™) I/O connections from the GuardLogix® area controller on the left, with various requested packet interval (RPI) settings, over the 5G core and RAN to the FLEX 5000 standard and safety I/O in areas 1 and 2 on the right. The RPI is the period at which the controller and the distributed I/O modules exchange data.

The test successfully demonstrated that the current state of industrial 5G (3GPP release-15, SA, on-premise, CBRS spectrum) has low enough latency and jitter to support RPI settings better than Rockwell Automation’s default settings for EtherNet/IP standard and safety I/O connections. These RPI settings will support many untethered stationary industrial asset applications (skids, machines or equipment) that use EtherNet/IP standard and safety I/O communications. Importantly, aside from typical IP address assignment and network setup, no special tuning or configuration was needed on the Nokia equipment; everything worked “out of the box.”

Using the CBRS spectrum helps ensure interference-free operation for critical automation equipment, maintaining uninterrupted performance. A private network with on-site hardware keeps data on premises, minimizing latency and enhancing privacy and security. Additionally, private cellular uses SIM cards, simplifying device management on your network.

Standalone (SA) 5G networks operate without a legacy LTE network, reducing costs and complexity while providing faster connections. As a result, using 5G for all network traffic (control plus user data) greatly reduces initial connection and handover times. For use cases requiring both 5G and LTE, LTE can be integrated with 5G SA networks.

Key use cases for private 5G SA include:

  • Edge-to-cloud connectivity: 5G’s low-latency, high-speed connectivity enables real-time data transmission and reliable coverage for AI and ML applications.
  • Connected worker applications: 5G’s excellent coverage and bandwidth enhance mobile tools like analytics, digital twins, and AR.
  • Mobile asset applications: 5G SA’s fast handover times and low latency improve connectivity for Automated Guided Vehicles (AGVs) and Autonomous Mobile Robots (AMRs).
  • Untethered stationary industrial assets: 5G reduces the need for wired communications, increasing agility and reducing retooling time for industrial operations.

Outside the US, industrial private wireless networks often use licensed spectrum. The performance observed with CBRS is consistent with results using other licensed sub-6 GHz bands as used in other countries, making these findings globally applicable.

Interested in learning more? Join us at the Rockwell Automation Fair in Anaheim, California, this November to experience our collaboration in action! Click here for further details about this event and how to register.

Automation Fair
Automation Fair
Event
Event
Automation Fair
Join more than 14,000 problem-solvers, makers and leaders for inspiration, connections and education at the 2026 Automation Fair® event.
Learn More

Published September 18, 2024

Topics: Empower People Networks & Infrastructure Process Solutions Solutions for OEMs Industrial Network Products

Scott Griffiths
Scott Griffiths
Advanced Technology Lab Manager, Rockwell Automation
Dr. Scott Griffiths has been with Rockwell Automation (RA) for six years and presently manages RA’s Advanced Technology team in Milwaukee. During his tenure in Advanced Technology, Dr. Griffiths was a senior researcher focused on industrial communications. In this capacity he studied 5G and co-led the execution of several collaborative testing efforts with 5G vendors. Dr. Griffiths is a subject matter expert on 5G within RA but has also worked on other research activities related to single-pair Ethernet, low-power wireless, and wireless power. Dr. Griffiths holds bachelor’s degrees in physics and mathematics from Oregon State University. His PhD is in experimental physics from the University of Iowa, where he developed low-energy X-ray polarimeters and studied gamma-ray astronomy. Prior to joining RA, Dr. Griffiths completed a post-doctoral fellowship in Spain, where he contributed to the construction of a prototype Large Size Telescope for the Cherenkov Telescope Array gamma-ray observatory.
Connect:
EmailEmail
Matt Hoover
Matt Hoover
Global Product Manager, Wireless and IIoT Products, Rockwell Automation
Matt’s career in software and technology includes leadership, sales, marketing, and development roles with Rockwell Automation, Linear Technology, Wind River, and Embedded Planet. In addition, Matt has extensive experience helping customers define and implement wireless IoT product solutions to realize digitalization and Industry 4.0 goals. Matt earned a Bachelor of Science in Mathematics / Computer Science from Kent State and an MBA from John Carroll.
Connect:
EmailEmail
Evan Forrest
Evan Forrest
Enterprise Partner Manager, Mobile Networks Americas, Nokia
Evan Forrest is the Enterprise Partnership Manager for Mobile Networks at Nokia, responsible for growing strategic technology and go-to-market partnerships. He joined Nokia in 2020, focusing on the establishment and expansion of Nokia’s industrial partner ecosystem across North America leveraging 4G/5G technologies. His role has evolved to leading lighthouse partnerships/projects across Transportation, Smart City, and Manufacturing sectors among others by way of enhanced digital connectivity. Prior to that, Evan spent 12 years in various sales and channel leadership roles at Rockwell Automation; helping manufacturers navigate Industry 4.0 and their digital transformation journeys. Evan earned his Bachelor of Science in Industrial Engineering from California Polytechnic State University - San Luis Obispo. Passionate about advancing digital solutions, he welcomes connections to discuss how manufacturers can harness 4G/5G for their digital transformation journeys.
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left Digital Transformation through 5G standalone (SA)
Please update your cookie preferences to continue.
This feature requires cookies to enhance your experience. Please update your preferences to allow for these cookies:
  • Social Media Cookies
  • Functional Cookies
  • Performance Cookies
  • Marketing Cookies
  • All Cookies
You can update your preferences at any time. For more information please see our {0} Privacy Policy
CloseClose