Loading
Blog
Recent ActivityRecent Activity

Is Your Machine Built for Thin Clients?

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Is Your Machine Built for Thin Clients? hero image

A great paradigm shift is occurring across much of the industrial landscape. As virtualization and thin-client technology have matured, more manufacturers are minimizing their reliance on highly-distributed computing in favor of a more centralized approach.  

In some ways, this transition reflects the classic “what was old is new again” scenario. Before the rise of personal computers (PCs), manufacturers accessed computing power via “dumb terminals” linked to mainframes. The terminal, which did not have an operating system, was simply a means to access the processing power of the mainframe.

However, this approach was supplanted by powerful PCs with expansive memory, impressive processor speeds and user-friendly interfaces. As a result, today most plant floors are characterized by a complex network of expensive to maintain desktop operating systems.

To better manage their processes, companies are increasingly taking a closer look at industrial thin clients that minimize reliance on PCs. Much like the dumb terminals of old, thin clients do not have hard drives or operating systems – but are built to provide remote access to servers where the processing power resides.

Using modern network technologies and powerful software tools, companies can enable secure, centralized configuration and delivery of applications and content from the server to every PC, thin client, mobile device and user.

And companies that are transitioning to thin-client platforms are expecting OEMs to deliver machines that can play in this environment.

It’s About Efficiency, Simplicity & Security

For both end users and machine builders, making the shift to thin clients for content management delivers significant benefits.

For end users, reducing the number of operating systems lowers the total cost of ownership substantially. There are fewer software licenses and less hardware to purchase and maintain.

Centralizing the content also simplifies application and device management for end users and machine builders alike. Deploying a new application or patch to a server-based system is more efficient than executing the update on multiple PCs across a multi-machine production line.  

Thin-client technology also inherently improves system security. While secure content is accessible via a thin client, all data and programming information is managed and stored on the server.

For both end users and machine builders, making the shift to thin clients for content management delivers significant benefits.

Therefore, content can only be modified through the centralized server – it cannot be accidentally or maliciously breached from a thin-client device.

For additional security, USB ports can be disabled and the Windows desktop can be eliminated.

Opportunities for Differentiation: “Machine Hyper-visualization”

A thin-client architecture also provides the framework for expanded ways to visualize machine content – and thereby differentiate a machine.

For example, this content delivery and visualization platform enables various thin-client terminals to shadow each other – so specific machine content can be more easily viewed anywhere within The Connected Enterprise®.

In addition, the platform can aggregate multiple content sources that can be visualized simultaneously on one thin-client device. Content from Windows-based applications, IP cameras, machine HMIs and more can be viewed using tiling or virtual screening to provide a truly comprehensive view of machine performance in real time.  

Imagine having multiple displays – like those available in a multi-screen control room – consolidated and accessible on your smartphone or tablet.

How Thin Clients Impact Machine Design & Deployment

So how does a thin-client paradigm impact machine design? Historically, OEMs have approached their machines as self-contained units, with application content managed locally on or near the machine. Transitioning to a thin-client platform requires a fundamental shift to a “centralized” mindset for machine content and storage.

In reality, most machine builders will be able to respond to specifications and execute machine design and development in the same way they always have.

However, OEMs must rethink their approach to the factory acceptance test (FAT) and site acceptance test (SAT) in a thin-client environment.

For the FAT, OEMs must simulate the server environment to verify the functionality of their system. Take a look at how this system integrator successfully implemented an FAT using a simulation system and proof of concept demo in a validated environment, successfully executing thin client site implementation.

Learn more about industrial thin-client hardware and software solutions.

Published June 11, 2018


Thomas Jordan
Thomas Jordan
Marketing Lead for ThinManager, Rockwell Automation
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left Is Your Machine Built for Thin Clients?