Loading
Blog | Digital Transformation
Recent ActivityRecent Activity

Is Patience Always a Virtue?

Start your digital transformation journey with a rapid-results asset performance monitoring tool to work smarter and prevent failures before they happen.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Asian businessman watching hologram screens. GUI (Graphical User Interface).

Maybe this is a peek into your future, or maybe it reminds you of the past, either way let us imagine you are starting your digital transformation journey and have identified an initial project to optimize asset availability. One way this will be achieved is to provide your maintenance teams with an asset monitoring tool to enable them to work smarter and proactively identify machine failures before they occur.

Some questions to ask yourself:

  • Do I look at multiple vendors, considering the many moving parts across many locations that may or may not be more than I really need?

Or,

  • Do I search for a solution that is specific to my needs; one that is fit for purpose that I can deploy fast and without losing valuable time?

It may appear that the answer is obviously the second choice, but you would be surprised how many companies take the first route. Perhaps you are one of them.

Digital Transformation
Digital Transformation
Digital Transformation
Explore how digital transformation can elevate your business, enhance efficiency, and drive innovation in today’s competitive landscape.
Learn More

Let’s consider the first option and what it entails.

  • First, you will need to talk with multiple vendors (possibly over many meetings) to assess their capabilities and find one that matches your needs.
  • Then you need to design the solution, map the requirements, agree on the system architecture, and so on.

All this takes time and don’t forget you will also need to allocate time to develop and implement the solution.

  • Then you will need to produce a plan on how to deploy across your different facilities and maybe even continents.
  • Was the need to have it available in local languages a requirement at the start?
  • Or maybe you missed one of a dozen other requirements that only manifest themselves after the solution is delivered into the hands of the users who will use it?

There is another way, the second option.

You might look for a product that is designed specifically for asset performance monitoring. In other words, a fit for purpose solution. This allows you to:

  • Skip the design stage
  • Reduce the development stage as it is more a case of configuration, and there are proven methods to deploy across multiple installations.
  • And when you identify the next use case on your digital transformation journey, and I feel confident saying that that is an inevitability, then you will be repeating the full process again to find the best solution.

Don’t get me wrong, both the above options have their advantages but maybe you should consider a third option:

One where you can combine the advantages of the other two.

One where you can get a ready-made asset performance monitoring solution meaning you can get results fast and one that allows you to add additional use cases when you are ready to take the next step in your journey.

If this sounds interesting, then check out our Out-of-the-Box IIoT Applications for Rapid Results webinar.

Sure, good things may well come to those who wait but hey, you do not always have to!

Published July 3, 2022

Topics: Accelerate Digital Transformation

Salma Ghafoor
Salma Ghafoor
Manager, Global Technical Lead – IOT, Rockwell Automation
Salma is a Global Innovation Leader focusing on edge and IoT at Rockwell Automation. She has over 25 years of experience working with information software and has a passion for understanding and sharing the benefits that IoT can bring to the industrial space.
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left Is Patience a Virtue in Digital Transformation?