Loading
Blog
Recent ActivityRecent Activity

How Manufacturers are Unlocking the Value of Data

Share This:

LinkedInLinkedIn
TwitterTwitter
FacebookFacebook
PrintPrint
EmailEmail
How Manufacturers are Unlocking the Value of Data hero image

For today's manufacturers, data is every bit as important as supply chains, trucks, and industrial machines. Data is useless if you don't turn it into insights — and then leverage that real-time information for new efficiencies, services, and business models. Digital transformation — technology change and organizational change — enables the agility that manufacturers will need to compete effectively.

Recently, I had the privilege of exploring how manufacturers are approaching digital transformation on a podcast with Scott Lapcewich, Vice President and General Manager of Customer Support and Maintenance for Rockwell Automation.

Here are some highlights from our conversation (Note - this transcript has been edited due to space limitations).

How Do Successful Manufacturers Start Going Digital?

Scott and I agreed quickly that it's important to get back to the basics when thinking about going digital – you need an actual plan! Many of the customers that we engage with are excited about the possibilities of digitization and we encourage them think about how their manufacturing operations fit into their overall business goals.

Scott brought up a few additional considerations following the development of your plan:

  • An outcome of that plan should include what investments are required from both an infrastructure and a modernization standpoint
  • Once you get connected and your plants are integrated, your data can be captured through an enterprise software application. At Rockwell Automation, we did this with our own plants and use our data to improve output and improve quality.
  • Finally we suggest integrating your manufacturing operations with both the front end of your business and the back end. Align your customers as well as your suppliers, so you can begin to optimize your responsiveness, inventory and production.

So Scott mentioned data. From my experience working with customers and even internally, data scares people. That includes the volume of data and what it's trying to tell them. Data for data's sake doesn't make sense. The sensor and the data together are powerful.

What Advice are You Giving Manufacturers to Optimize Performance?

As I said previously, first you need to unlock the data that exists so you can actually start reacting to what's going on. Looking at what's there can be scary because if it's not there and you can't see it, it's a great way to hide problems.

When I look at the numbers of sensors coming out and talking, some surveys are 20 billion sensors in the next five years, some are 40, some are 50, but the number doesn't matter. It's a huge amount of data from those sensors. What we need to talk about is where did the data come from, what we do with it, how do we do it, and where are you looking at it from. We also need to help our customers understand that data, how they're either using or not using the data, and how to prioritize that information.

Scott gave some examples of what Rockwell Automation is doing to indicate the health of different assets and generate automated diagnostic information on what's happening on the plant floor. By building automated analytics into Rockwell Automation programmable controllers and enterprise software, customers can get intelligence coming back from the machines.

We also talked about the significant opportunity to analyze data trends and monitor performance benchmarks to help customers determine specific actions they can take within their operations. As an example, to improve quality they can view long-term trended data to pinpoint what factors may lead to declining quality over time.

How Can They Master (or Get Control of) Their Data?

One thing we always hear from manufacturers is they are getting data and dashboards, but the problem is they have too much data and not enough expertise around the alerts being received. If an alert goes off, they want built-in workflows to call the expert – whether in-house or out.

I asked Scott if Rockwell Automation is building any capability that routes the alerts on devices to a trained operations professional so that customers can start handing it off to automation suppliers.

Turns out it's not as easy as it may sound. He explained that the challenge is there's a lot of alarms that occur in a process line in any given day. Some of them are meaningful, some are not.

So in terms of being able to set up a managed service agreement with customers, there needs to be collaboration up front as to what the process line is doing, what the key variables and trends are, and how to monitor them to indicate potential issues. Then you can set up the sensors and monitoring capability to identify which combinations of events or alarms indicate a potential pending failure, pending issue, or an issue that's already occurred.

Rockwell Automation does in fact provide the service of routing alarms to their support center where someone is available to respond 24 hours a day. They can also route alarms directly to a specific domain expert's desktop – wherever they are in the world – to troubleshoot remotely.

Those are a few of the key takeaways from our discussion. Listen to the full podcast here and check out our slideshare for more high-level takeaways.

This blog was co-authored by Scott Lapcewich, vice president and general manager, customer support and maintenance, Rockwell Automation.

Published June 30, 2016


Doug Bellin
Doug Bellin
Global Senior Manager, Manufacturing and Energy, Cisco
Connect:
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
  • Customer Care
  • TechConnect Support
  • General Questions
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right