What has changed in the UL508A third edition? What are the implications on the panel?
Have questions on short-circuit current ratings?
This webinar will provide examples for short-circuit current ratings of panels based on the methods stated in UL 508A Supplement B. While other standards require short-circuit ratings, this webinar focuses on UL508A SB4 and SB5, short circuit and panel marking.