Configure the Primary Controller
Configure a program for only the primary controller. Both primary and secondary controllers use the same controller program. You do not need to create a separate project for each controller.
IMPORTANT:
Unless a workflow dictates that the controller in the secondary chassis requires modification, only interface with the primary controller.
Provide Feedback