Reset Factory Defaults
On the Configuration tab in the
FactoryTalk® Linx
RMCT, you can reset the redundancy module to its factory defaults when the redundant chassis pair is in a disqualified state.After a reset, the following settings are restored on the redundancy module.
Setting | Default |
|---|---|
Module identification information (name, description, location) | Blank |
Auto-synchronization | Conditional |
Auto-synchronization state | Enabled |
Chassis ID | Chassis A |
Enable User Program Control | Disabled |
Enable Fiber Security | Enabled |
Reset to Factory Defaults

Provide Feedback