Disable CIP Security Ports via FactoryTalk Linx

To disable
CIP Security
ports via
FactoryTalk® Linx
, complete the following.
  1. If the Device Configuration menu in
    FactoryTalk® Linx
    is not enabled, go to the Advanced Settings dialog box and check the Enable Device Configuration checkbox.
    This image shows where to enable/disable device configuration in FactoryTalk Linx.
  2. From the Device Configuration menu, click the CIP Security tab, and then check the Disable CIP Security (Port 2221) checkbox.
    This image shows where to disable CIP Security on a port in FactoryTalk Linx.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal