Metal Form Instructions
    AVC  | Name  | Description  | 
|---|---|---|
AVC  | Auxiliary Valve Control  | Controls an auxiliary valve that is used with a main valve.  | 
CBIM  | Clutch Brake Inch Mode  | Used for press applications where minor slide adjustments are required, such as press setup.  | 
CBCM  | Clutch Brake Continuous Mode  | Used for press applications where continuous operation is desired.  | 
CBSSM  | Clutch Brake Single Stoke Mode  | Used in single-cycle press applications.  | 
CPM  | Crankshaft Position Monitor  | Used to determine the slide position of the press.  | 
CSM  | Camshaft Monitor  | Monitors motion for the start, stop, and run operations of a camshaft.  | 
EPMS  | Eight-position Mode Selector  | Monitors eight safety inputs to control one of the eight outputs that correspond to the active input.  | 
MMVC  | Maintenance Manual Valve Control  | Used to drive a valve manually during maintenance operations.  | 
MVC  | Main Valve Control  | Controls and monitors a main valve.  | 
Provide Feedback