Set Home Position
The Set Home Position command sets the current position of the axis as the new Home
Position. There is no movement of the axis.
Tag Name | Data Type | Description |
|---|---|---|
Command Tags | ||
O.Axisxx.Command_SetHomePosition | BOOL | Indicates that the axis is to perform the Set Home Position
command. |
O.Axisxx.HomePosition | REAL | Specifies the position value to set as the current position. This value is an offset to use as the home position, not the actual
physical position of the axis. If the home switch is not at the zero
position, you can use this tag to set the offset from the zero
position. |
Set Home Position Timing Diagram – When Home Position is Zero
Set Home Position Timing Diagram – When Using an Offset for Home
Position
Provide Feedback