Direction
The
I.SSIxx.Direction
tag indicates the sensor position direction as per the last
SSI sensor movement. Every sampled SSI sensor data (after filtering) is compared with
the previous sample to determine the direction. 0 means that the position is moved up. 1
means that the position is moved down.Provide Feedback