Count/Internal Direction Mode
In this mode, the
O.Counterxx.Direction
tag determines the direction of the
counter.Invert Counter Direction Setting | O.Counterxx.Direction Tag | Input A (Count) | Input B (Not Used) | Change in Count Value |
|---|---|---|---|---|
Disabled | 0 | Rising edge | – | 1 |
1 | Rising edge | -1 | ||
Enabled | 0 | Rising edge | -1 | |
1 | Rising edge | 1 |
Provide Feedback