No Load Diagnostics

No Load Diagnostics detects when a signal wire is disconnected from an output channel. When the
I.Ptxxx.Fault
tag is set to 1, check the channel diagnostic or retrieve the information from the diagnostic assembly to verify that the No Load condition is present.
You can only configure channels 1, 3, 5, and 7 as “Digital Output, Short Circuit, No Load”.
To enable No Load Diagnostics, see Chxx - Digital Output View.
For more information on how to retrieve diagnostic assemblies, see Diagnostic Assembly.
For more information on using module tags, see 5034-IOL4 and 5034-IOL4XT Details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal