Construct a PointMax I/O System

PointMax I/O system contains the components that are pictured below.
PointMax I/O System
Item
Component Name
Description
A
Adapter
The adapter transfers data between the I/O module and the controller.
B
Removable Terminal Block (RTB)
The RTB contains terminals to terminate wiring for field devices. Also it has interfaces to establish the connection between the RTB and the I/O module.
C
I/O module
The I/O module contains the SA or field power interface and circuitry that is needed to perform specific functions that are related to your application.
D
Mounting Base (MB)
The MB contains mechanical and electrical interfaces to establish the connection between I/O module and the backplane.
E
End cap
It is a dust protection cap for the last module in a rack.
For PointMax I/O system power requirements, see PointMax I/O System Installation Instructions, publication 5034-IN001.
IMPORTANT:
You must limit the SA field-side power source to 10 A max, at 20...30V DC.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal