Configure Channel Output State When Module is in Program Mode or Inhibited
You can configure individual output channels to specific states when the IO-Link master
module is in Program mode or when the module is inhibited.
When the controller switches from Run mode to Program mode, the output can behave in the
following ways, depending on how you configure the Output State in Program Mode
parameter:
- Turn off - Default
- Turn on
- Hold its last state
When the IO-Link master module is inhibited, the output behavior follows the Output State
in Program Mode configuration.
To configure the output states in Program mode or when the module is inhibited, see Chxx - Digital Output View.
Provide Feedback