Import/Export IODD Files

You can export the IODD files of the devices that you are using in your application to share with others to help make sure that everyone uses the same device descriptions when working across multiple systems.
For example:
  • You can export the IODD files for the devices that are used in your machine into one file and provide it to your customers so that they can use the same devices and IODD file versions in their configuration.
  • If you are collaborating on a project and you have unidentified devices in your setup, you can import the shared IODD files into your system to help make sure that you are working in the same programming environment.
Use the Device Description File Installation Tool, which is installed along with FactoryTalk Linx software, to import and export the IODD files of your devices.
To import or export IODD files, see Import/Export IODD Files.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal