Replace with a Used Master Module when any Device DS Backup/Restore Enabled and ADC Disabled

To replace an IO-Link master module in this scenario, complete these steps.
  1. In the IO-Link master Module Properties → Connection view, select the Inhibit Module checkbox and select Apply.
  2. Replace the IO-Link master module.
  3. In the IO-Link master Module Properties → Chxx - IO-Link view, select Disable and Delete Data Storage to delete the IO-Link storage. Repeat this step for all IO-Link channels.
    IMPORTANT: You must clear all local Data Storage copies to prevent the device configurations from being overwritten by the Data Storage in the used IO-Link master module.
  4. In the IO-Link master Module Properties → Connection view, clear the Inhibit Module checkbox and select Apply.
    The device configurations are backed up to the replacement IO-Link master module when device connections are established.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal