Hold for Initialization

Hold for Initialization causes outputs to hold present state until the value commanded by the controller matches the value at the output screw terminal within 0.1% of full scale, providing a bumpless transfer.
If Hold for Initialization is selected, outputs hold if there is an occurrence of any of these three conditions:
  • Initial connection is established after power-up.
  • A new connection is established after a communication fault occurs.
  • There is a transition to Run mode from Program state.
  • The module loses SA power. In this case, the data echo value goes to 0.0.
The
I.Chxx.InHold
tag for a channel indicates that the channel is holding.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal