Point Power Supply
You can configure the 5034-UB8 and 5034-UB8F module points to function as a power
supply.
Typically, for points that are configured as an input (Digital Input, Digital Input –
Timestamp, Digital Input – Counter, or Digital Input – FIFO), you can select the power
source as External Power Supply, Module SSV, or Point in Power Supply mode. When the
point that is configured as a power supply is faulted, the fault bit of that input point
is also set.
Input Point Power Source Example
Provide Feedback