Field Power (SA Power) Loss Detection

IMPORTANT:
This feature is not applicable to 5034-IA8/XT module.
The Field Power Loss Detection feature monitors for the loss of field-side power on the SA power bus.
In the diagnostic assembly, the FieldPowerOff bit is set at the module and point level structure. The Fault bit is set at the point level.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal