Connect to the EtherNet/IP Network

You must set the network address on the adapter for the adapter to operate on an EtherNet/IP network.
The following are adapter conditions in which you set the network address:
  • Set the network address for the first time after it powers up in the out-of-box state.
    IMPORTANT:
    The adapter powers up in the out-of-box state the first time you install it.
  • Change the IP address after it has been set.
    IMPORTANT:
    Verify that the network address for the adapter is not a duplicate of any existing devices on the network.
Requirements
To set the network address, have the following:
  1. The MAC ID that is located below the QR code on the adapter
  2. The recommended IP address for the adapter
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal